The impact of population growth, water scarcity and climate change on water availability is substantial. Reused water is the most sustainable water source, consuming four times less energy compared to desalinated sea water. The Safi Water Recycling Plant is a unique facility in Ajman, UAE where up to 13,000 cubic meters per day of treated wastewater is polished to very high-quality standards.
Our solution
Reliable, accurate and robust electromagnetic flow meters for process monitoring and billing applications
Inline monitoring of critical quality parameters at both the inlet and outlet of the reverse osmosis membranes
Ensure membrane cleaning efficiency
Reduced total cost of ownership (TCO)
Local support and service expertise
“The collaboration with Endress+Hauser has paved the way to a more sustainable water future. Easy asset management for maximized sensor lifetime and local expertise have contributed to a lower TCO.”
Habib ur Rahman, Plant manager
Safi, United Arab Emirates (UAE)
Customer challenge
As a responsible operator, Safi continuously monitors various parameters to ensure that the permeate water quality always meets the stringent requirements set by the End users industries. Water reuse often involves advanced treatment processes such as membrane filtration and reverse osmosis. Managing these complex treatment steps requires manpower, the availability of skilled personnel and substantial investments.
Realization
Ultrafiltration and reverse osmosis membranes are prone to fouling and scaling which occurs when dissolved and undissolved particles and minerals as well as microorganisms accumulate on the membrane surfaces, reducing permeability and energy efficiency. Optimal monitoring of critical parameters ensures initiating timely chemical cleaning and backwashing cycles which are critical to prevent flux degradation and prolong membrane lifespan and its replacement.
Safi operates and develops wastewater reuse assets for the Emirate of Ajman. The company manages public infrastructure as a profitable environmental manner that fulfils the high standard of sustainability that lies at the heart of the Ajman Government’s values.
As a winner of the coveted Global Water Awards for “Water Reuse Project of the Year 2012”, the plant is the first branded water reuse operations in the world.
Tarayıcı deneyiminizi iyileştirmek, site işlevselliğini optimize etmek adına istatistikleri toplamak ve size uygun reklam ve içerikler göstermek için çerezleri kullanıyoruz.
"Tümünü kabul et" seçeneği ile çerez kullanımımıza rıza göstermiş olursunuz.
Daha fazla ayrıntı için lütfen göz atın: Çerez Politikamız .