Digitalization simplifies the collection and monitoring of energy data
In order to uncover and realize the savings potential available in the utilization of steam, water and air pressure in line with the brewery’s environmental goals, Hofbräuhaus installed an energy monitoring system, which relies on digitalization, with the support of Endress+Hauser.
The results
Regardless of the product, continuous monitoring ensures fully transparent energy utilization, from brewing to filling
Thanks to digitization, monitoring was simply integrated into the existing infrastructure
With the FieldXpert I have simple and fast mobile access to the current energy utilization data from anywhere, plus I can analyze trends and configure the instruments.
Silvio Di Tano, Head of Electronics
Staatliches Hofbräuhaus München
Customer challenge
The state-owned brewery wants to sink the specific heat consumption by 4 percent and production-generated CO₂ emissions as much as 30 percent. All of the individual measures will be bundled into an environmental management system. An automation concept for the integration of the data had to be developed. This concept is designed to ensure the seamless collection of energy utilization data and provide mobile access to the data.
Our solution
Heart of the solution is Memograph M, a data manager that serves as an interface between the field instruments and the process control level. Memograph M forwards the actual sensor measurement values to the control system via PROFINET. Mobile access to the energy data monitoring system is fulfilled by the FieldXpert. This robust industry-scale tablet PC features a preinstalled device driver library for all important protocols and automatically detects instruments with a click.
Bira fabrikasının çevresel hedefleri doğrultusunda buhar, su ve hava basıncının kullanımında mevcut tasarruf potansiyelini ortaya çıkarmak ve tasarrufu gerçekleştirmek için Hofbräuhaus, Endress+Hauser'ın desteğiyle dijitalleşmeye dayanan bir enerji izleme sistemi kurdu.
Tarayıcı deneyiminizi iyileştirmek, site işlevselliğini optimize etmek adına istatistikleri toplamak ve size uygun reklam ve içerikler göstermek için çerezleri kullanıyoruz.
"Tümünü kabul et" seçeneği ile çerez kullanımımıza rıza göstermiş olursunuz.
Daha fazla ayrıntı için lütfen göz atın: Çerez Politikamız .